Test passed - levitation technology project uses screws from norelem
Award-winning levitation technology: the muZero hyperloop project from the Karlsruhe Institute of Technology has won second place in the ‘Complete System’ category at the European Hyperloop Week 2024 in Zurich. The guidance system with its specially developed software solution impressed the jury. Since 2020, alternating project teams have been working on the innovative high-speed transport system, continuously supported by expertise and components from norelem.
The muZero Hyperloop is the prototype of a rail-guided transport capsule with an electromagnetic levitation system. The capsule reaches speeds of up to 109 km/h. Finally, the interaction between the pod (transport capsule) and the track (route or rail on which the pod moves) was further optimised and the guidance system eventually won an international award. The main task of the track is to provide the pod with a stable and safe environment that ensures controlled operation. In order to test the hovering system in practice, an 11 metre long test track made of standard steel profiles was constructed.
These were securely connected using various hexagon head bolts, matching hexagon nuts, washers and swivel feet from norelem. The bolts can be easily loosened again if required in order to transport the test track. They are also strong enough to withstand the forces and movements that occur. The countersunk screws, which are located in the track of the pod, are particularly important here. Their heads are flush with the surface. This prevents the pod from colliding with protruding screws and thus being damaged or disturbed while travelling. The screws also enable precise adjustment of the individual components so that the rails can be precisely aligned.